Ugrás a fő tartalomra Ugrás a kereséshez Ugrás a fő navigációhoz
Üdvözöljük az újonnan felújított weboldalunkon!

Shopbox

Shopping trolley castors with a significant asset: sustainability.
shopbox_banner
A single shopping trolley covers thousands of kilometres in ten years of service life. It thus needs castors that endure significant wear and tear.
When carrying out necessary maintenance, the aim should be to conserve valuable resources and reduce the burden on the environment. For this reason, we provide our customer ShopBox with shopping trolley castors that make it possible to replace only those parts that really need renewing. The result: improved sustainability and lower costs.

Szeretne személyes tanácsot kapni?

Várjuk megkeresését

Hans-Peter Vetvicka, General Manager of ShopBox Group GmbH

Hans-Peter Vetvicka, General Manager of ShopBox Group GmbH

With TENTE, we save two thirds of the costs and protect the environment.

Hans-Peter Vetvicka, General Manager of ShopBox Group GmbH

Conserving resources and saving costs

Our solution is valued by ShopBox and its customers for its sustainability, ease of maintenance and cost efficiency. Not only are resources conserved and the burden on the environment noticeably reduced, but also two thirds of the costs are saved. With 40,000 serviced shopping trolley castors per year, this is a considerable advantage for ShopBox. In addition, the solution also improves the maintenance process because the wheel and fork can now be removed individually, making maintenance quicker, easier and more efficient.