Ugrás a fő tartalomra Ugrás a kereséshez Ugrás a fő navigációhoz
Üdvözöljük az újonnan felújított weboldalunkon!

P. Lindberg Industri A/S

Extra heavy-duty castors to carry a 108-metre rotor blade.
p_lindberg_industri_banner
Rotor blades for a wind turbine weigh more than 50 tons – as much as nine fully grown elephants. But our twin-wheel castor Omikron can handle it.
Our Danish customer P. Lindberg Industri A/S produces trolleys for transportation which must also be able to carry this weight capacity. This kind of trolley is used in the production of wind turbine blades. The rotor blade does not only need to be rotated easily but the trolley itself must be movable as well. Are TENTE castors able to carry this weight? Yes, of course!

Szeretne személyes tanácsot kapni?

Várjuk megkeresését

Lars Hansen, Managing Partner, P. Lindberg Industri A/S

Lars Hansen, Managing Partner, P. Lindberg Industri A/S

We are proud to contribute to climate protection with our trolleys when it comes to the production of rotor blades. Our supplier TENTE supports us with its reliability and the quality of the heavy-duty castors.

Lars Hansen, Managing Partner, P. Lindberg Industri A/S

Suppliers to the wind power industry: our contribution to climate protection

The transport trolleys from P. Lindberg Industri A/S consist of up to 1,000 individual parts. Elaborate engineering drawings ensure a stable and precise fit when it comes to the merge of the rotor blades and the trolleys. The welders take extra care with the numerous seams they weld. Non-destructive tests of the weld seams ensure quality, because with this weight, accidents would be devastating. Just like the production of the rotor blades, a lot of manual work is required because all trolleys are custom-made. TENTE also pays particular attention to the high quality of its castor production. Supported by its own specialist welding engineers and in cooperation with TENTE product developers and welding specialists, special care is taken to ensure the quality of the work while producing the components. Extensive tests and trials in the laboratory and at public testing institutes ensure the quality of TENTE extra heavy-duty castors. P. Lindberg Industri A/S and TENTE have been working together in a spirit of trust for 20 years. Both companies contribute to the wind power industry as they move together towards this industry of the future.