Ugrás a fő tartalomra Ugrás a kereséshez Ugrás a fő navigációhoz
Üdvözöljük az újonnan felújított weboldalunkon!

Marks & Spencer

Small castors – high loads. Our furniture castor Linea load makes this combination possible.
marks_spencer_banner
The decisive factors for presentation furniture in a merchandise stores are availability of space, flexibility and durability – at TENTE, we combined it all
Our globally active customer Marks & Spencer, based in the UK, relies on mobile shelves fitted with our extremely compact furniture castor Linea load. Their special feature: a dynamic load capacity of up to 100 kilograms with a diameter of just 50 millimetres.

Szeretne személyes tanácsot kapni?

Várjuk megkeresését

Alex Neilson UK & International Specification Manager at Marks & Spencer

Alex Neilson UK & International Specification Manager at Marks & Spencer

The Linea load is compact and highly resilient – simply ideal for our gondolas and rails.

Alex Neilson UK & International Specification Manager at Marks & Spencer

Maximum durability, operational safety and flexibility

Due to its compact dimensions, Linea load is ideal for the existing display fixtures used at Marks & Spencer and also improves the load capacity and safety. It thus opens up greater scope for the flexible use of the retail spaces and is a solution that the employees can rely on 100 percent. Marks & Spencer also benefits from this close cooperation on a global level. As a result of our global presence on five continents, we are able to respond very quickly and offer the retail company the best possible customer support at every one of its locations.