Salta al contingut principal Salta a la cerca Salta a la navegació principal
Benvingut al nostre lloc web redissenyat!

Interpane

Trolley castors safe enough for extra heavy loads.
interpane_banner
Transporting glass loads requires extreme caution. Especially when the loads take on the dimensions of a small bus.
Such a challenge calls for transport trolleys with extra heavy-duty castors that demonstrate outstanding manoeuvrability and guarantee the physical well-being of the employees. For the renowned glass manufacturer and processor INTERPANE, we have therefore developed a foot protection system that represents the highest level of work safety and at the same time enables trouble-free transport of glass panes.

¿Le gustaría recibir asesoramiento personalizado?

Esperamos recibir su consulta

Tobias Rüther, Corporate Safety Coordinator of the INTERPANE Group

Tobias Rüther, Corporate Safety Coordinator of the INTERPANE Group

With TENTE’s solution we have improved both occupational safety and the protection of our products.

Tobias Rüther, Corporate Safety Coordinator of the INTERPANE Group

Perfectly adapted safety

The new foot guard is available for wheels in four sizes, from 125 to 250 millimetres, and allows for quick and uncomplicated retrofitting of the trolleys for extra heavy-duty loads. During the development process, we naturally also considered the thermal conditions that play a role in the production and assembly of glass elements, and indeed in almost all other areas of industrial production. So, our mobility solution is suitable for use at minus 40 degrees Celsius and up to 80 degrees Celsius.