Skip to main content Skip to search Skip to main navigation

Casters for fire service roll containers:

Safe movement, reliable locking
Braun_Feuerwehrtechnik_TENTE_Customer_Reference_1
Fire service roll containers make sure hoses, firefighting and flood response equipment, breathing aids, and heavy-duty work and rescue equipment quickly get to where they are needed. They require transport casters that remain easy to steer even under heavy loads, perform reliably in demanding operating conditions, and keep the container securely in place at the incident site.
The TENTE Alpha product family provides robust, adaptable solutions for these requirements, with load capacities of up to 500 kg per caster and a choice of locking functions, wheel materials, and fittings.

What casters for fire service roll containers need to offer

Load capacity is not the only factor that matters during an emergency response. Fire service roll containers are moved frequently, loaded into and unloaded from vehicles, and exposed to changing environmental conditions. Smooth running and easy steering reduce the effort required. A reliable locking system prevents unintended movement and helps keep the container stable at the incident site. 

Alpha casters for reliable performance

Fire service roll containers need casters that reliably carry heavy loads, are easy to maneuver, and continue to operate safely in demanding conditions. 

Depending on the version, multiple Alpha casters can be locked or released simultaneously from a central control. Options are available with central wheel locking, directional locking, or total locking. This reduces operating effort and the risk of individual casters being left unsecured. The technical design – using profile bars, levers, or integrated solutions, for example – can be tailored to the construction and requirements of each fire service roll container. 

Get in touch

Would you like individual consultation for your specific application? Contact our TENTE experts today.

Versatile configuration options

Depending on the combination of wheel, housing, and fitting, the Alpha product family offers features including: 
  • Easy maneuvering: A swivel bearing with a double ball race supports precise steering.  

  • Robust design: Wear-resistant wheel variants withstand heavy use, while sealed bearings protect against splash water and dirt. 

  • Designed for the operating environment: Heat-resistant and corrosion-resistant versions are available. 

  • High load capacity: Depending on the wheel, housing, and fitting combination, the Alpha product family offers load capacities of up to 500 kg per caster. 

Skip image gallery

Our heat resistant casters

Learn more about the technical versions, fittings, and locking functions of our heat-resistant casters.

Practical example

Alpha casters at Braun Feuerwehrtechnik

Our partnership with Braun Feuerwehrtechnik demonstrates how the solution performs under real operating conditions. The company develops roll containers for fire services that carry hoses, firefighting equipment, flood response equipment, breathing apparatus, and heavy-duty work and rescue equipment. 

The roll containers are used in cold and heat, wind and rain, and snow and ice. The combination of high load capacity, easy maneuverability, central locking, and the dust guard on TENTE Alpha casters supports safe, flexible transport of equipment all the way to the incident site. 

Selected Alpha Castors

Selected Alpha castors at Braun Feuerwehrtechnik:

Wheel diameter: 8 in
Dynamic load capacity: 880 lb per caster
Caster configuration: Four Alpha casters per roll container, or six for particularly heavy containers
Locking system: Central locking

Thoughtfully engineered safety for heavy roll containers

The Alpha casters on the fire service roll containers are connected by a robust linkage. An operating handle transfers the hand movement through a gas spring to a second bar. This locks or releases all casters simultaneously without bringing the container to an abrupt stop. 

An additional dust guard on the swivel bearing limits sideways caster movement. This reduces the risk of tipping when the casters are locked – an important safety feature for heavy roll containers. 

— Thomas Braun, Founder and Managing Director of Braun Feuerwehrtechnik GmbH

— Thomas Braun, Founder and Managing Director of Braun Feuerwehrtechnik GmbH

We have worked closely together for years. TENTE always takes our challenges seriously. Together, we develop a solution precisely tailored to our customers, for whom safety is a top priority.

— Thomas Braun, Founder and Managing Director of Braun Feuerwehrtechnik GmbH

Braun Feuerwehrtechnik GmbH Case Study

Read how Braun Feuerwehrtechnik and TENTE jointly developed a safe, robust solution for fire service roll containers.

Which casters are right for your fire service roll container?

Load capacity, wheel material, fitting, and locking function must match the design, load, and operating environment of the roll container. Tell us briefly about your requirements.

Our experts will help you select and configure the right Alpha casters.

Fields marked with asterisks (*) are required.