When a supermarket is stocked using roll cages, it can soon become very noisy – but not with the right castors.
After all, intense noise is not only an unpleasant disturbance, but above a certain level also impacts health. The logistics specialist GEBHARDT therefore relies on our Syntech wheels. These wheels combined with their high load capacity are significantly quieter than ordinary wheels – ten decibels quieter, to be precise.
Norbert Götz, Purchasing Manager at GEBHARDT Logistic Solutions GmbH
For more than 30 years, we have been using TENTE’s professional expertise.
Norbert Götz, Purchasing Manager at GEBHARDT Logistic Solutions GmbH
Longer durability and reduced costs
The Syntech wheel has a service life more than twice that of hard-filled castors, which are used for an average of only two years. In contrast, the Syntech wheel is often used for up to five years. This saves costs both in purchasing and maintenance and is another decisive reason why GEBHARDT relies on long-term cooperation with our company.