W
What is meant by the resistance of wheels and castors?
  • Termékek
  • Szakterületek
  • Megoldás
Lexicon: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Kezdőoldal | Tartalomjegyzék
Lexicon navigáció
A B C D E F H I L O P R S T V W Kezdőoldal Tartalomjegyzék

What is meant by the resistance of wheels and castors?



Rolling and swivel resistance of castors 
 When you want to set a device in motion, you must first overcome the starting resistance. The manoeuvrability of the equipment thereafter is then influenced by the rolling and swivel resistance. The resistance depends on various factors, including: 
+Load 
+Wheel 
+diameter 
+Wheel material 
+Bearing type 
+Floor conditions 
The type, number and arrangement of the castors have an influence on manoeuvrability. A device that only needs to be moved straight ahead, for example, can be equipped exclusively with fixed castors. If steering is required, a combination of fixed and swivel castors or the use of swivel castors with a directional lock is ideal.
Electrical resistance 
The electrical resistance describes the electrical voltage required to allow an electrical current to flow through a conductor. Antistatic and electrically conductive castors and wheels from TENTE protect against electrostatic discharge. Electrically conductive castors and wheels have an ohmic resistance of less than 104 Ω. The ohmic resistance of antistatic castors and wheels is at 107 Ω. 
Electrically conductive castors and wheels are important in the medical field, for example, as electrostatic discharges can have far-reaching consequences. They are also frequently used in the industrial sector. TENTE’s meticulous quality control ensures that the wheels and castors meet the strictest requirements.