W
What are the advantages of a polyurethane tread?
  • Termékek
  • Szakterületek
  • Megoldás
Lexicon: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Kezdőoldal | Tartalomjegyzék
Lexicon navigáció
A B C D E F H I L O P R S T V W Kezdőoldal Tartalomjegyzék

What are the advantages of a polyurethane tread?

Polyurethane is ideally suited as tread material for castors & wheels

Polyurethane: A floor-friendly and robust tread
Polyurethane (PUR) is widely used as a tread material for wheels and castors. PUR has elastic properties and is also very robust. The material's robustness makes it ideal for castors and wheels that have to carry heavy loads.
The tread influences the smoothness of running, the starting, swivel- and rolling resistance and the overall drive comfort of a castor. The choice of tread depends, among other things, on the type of floor on which the castors are to be used. As a general rule, the tread should be softer than the floor so that the castors do not leave indentations or marks. 

Polyurethane wheel treads 
Polyurethane is a floor-friendly tread that is elastic, abrasion-resistant and exceptionally resistant to many substances. Treads made of PUR are also characterised by low rolling resistance and therefore excellent drive comfort. At particularly high or low temperatures, however, polyurethane is not the preferred solution. In this case it is possible that the load carrying capacity decreases and the rigidity increases. 
We can help you find the right tread for your castors and wheels, whether polyurethane, rubber, stainless steel or any other material. Please contact us. If you have any questions about our products or require an individual special solution, our expertise and experience are at your disposal.