W
What are the advantages of a rubber tread?
  • Termékek
  • Szakterületek
  • Megoldás
Lexicon: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Kezdőoldal | Tartalomjegyzék
Lexicon navigáció
A B C D E F H I L O P R S T V W Kezdőoldal Tartalomjegyzék

What are the advantages of a rubber tread?

The tread material has a profound influence on the quality of a castor or wheel.

Rubber treads on TENTE castors and wheels 
It influences the smoothness of running, the resistance, the starting, rolling and swivel resistance – and the drive comfort of the castor or wheel. The category of rubber treads covers a large group of possible treads: These include solid rubber, thermoplastic rubber, a special hard soft rubber and pneumatic tyres.
As a rule of thumb: The tread should be softer than the floor on which the castors are used. Otherwise, the wheels may press into the floor and damage it. One exception is the use of wheels on soft floors such as carpets: A wheel with a hard tread can also be used here. 

Advantages of a rubber tread 
Rubber surfaces have in common that they are usually extremely kind to floors and also dampen vibrations. They have low swivel and rolling resistance, which means excellent drive comfort. Another advantage is the material's resistance to many aggressive substances. Solid rubber, for example, can be used almost universally. Heat-resistant solid rubber tyres can be used even at extreme temperatures above 200 °C. Thermoplastic rubber is non-marking and runs quietly. However, this material cannot be used in the high temperature range.
Pneumatic tyres are also made of rubber. Their rolling resistance is low even on difficult floors. In the case of pneumatic tyres, it is important to maintain the specified tyre pressure at all times. Regular pressure testing ensures that the tyres are functional in the long term. 
We can help you choose the best material for the treads of your castors and wheels. Whether it be rubber, polyurethane or any other material – we will find the solution that makes your application run smoothly!