W
What are the advantages of central locking?
  • Termékek
  • Szakterületek
  • Megoldás
Lexicon: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Kezdőoldal | Tartalomjegyzék
Lexicon navigáció
A B C D E F H I L O P R S T V W Kezdőoldal Tartalomjegyzék

What are the advantages of central locking?

A central locking mechanism locks several castors at once and thus effectively immobilises the transport equipment and prevents it from rolling away or shifting. In contrast to individual locks, this system is connected to at least two castors, and can also directly affect all of the castors. Central locking is useful for all applications where equipment has to be constantly moved and stopped again.

Advantages of central locking 
The biggest advantage of a central locking system is obvious: Multiple castors can be locked or released at once. Depending on the system, the locking mechanism can be operated by hand instead of with the foot. The ergonomic benefit of this for the operator should not be underestimated. Furthermore, the lever for the central lock is always located at the same position on the equipment. If the equipment is fitted with individual locks, on the other hand, it is possible – depending on the wheel position – that the operating elements may be located underneath the equipment. For safety purposes, the lever of a central locking system can also be protected by means of a lever lock, if required. 

Applications for central locks 
An example of use: Hospital beds can be equipped with a locking system that acts on all four swivel castors simultaneously. The castors are released or locked by a pedal. It is also possible to fix two castors in the straight-ahead position to make it easier to push the bed in a straight line. The lock can be operated from both sides of the bed. As a general rule, central locking is recommended in all situations where it is important to be able to fix the equipment securely in a stationary position and to operate the locking system quickly, easily and reliably. In addition to hospital beds, waste containers are another typical type of application. We will be happy to discuss whether a central locking system is worthwhile for your application. Contact us and let TENTE’s experts advise you on all aspects of this topic!