W
What are thermoplastic elastomers?
  • Termékek
  • Szakterületek
  • Megoldás
Lexicon: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Kezdőoldal | Tartalomjegyzék
Lexicon navigáció
A B C D E F H I L O P R S T V W Kezdőoldal Tartalomjegyzék

What are thermoplastic elastomers?

Thermoplastic elastomers (TPE) are plastics that combine the material properties of classic elastomers with the processing advantages of thermoplastics. This means that they behave like elastomers at room temperature and like thermoplastics when heated. As a tread material for wheels and castors, we have developed TENTEprene, a thermoplastic rubber with particularly good running properties.

Supratech tread material - Thermoplastic rubber for castors 
Supratech is very kind to floors and offers high running comfort. The tread is very quiet and leaves no marks on the floor. It is also easy to clean and can therefore be used in areas where hygiene is subject to strict regulations. Castors with TENTEprene treads are characterised by low rolling and swivel resistance and are therefore also very easy running. Especially in combination with high-quality precision ball bearings, this thermoplastic rubber is suitable for carrying heavy loads. Even when supporting heavy weights, the wheels run smoothly and are easy to manoeuvre. 

Applications for TENTEprene 
Thanks to its properties, a castor with a tread made of TENTEprene thermoplastic elastomer can be used in many areas. Since the castors are washable, they can be used wherever hygiene is of great importance, for example in hospitals or in the food industry. In addition, their high load-bearing capacity makes them the ideal choice for transporting heavy loads. At the same time, the tread is easy to manoeuvre and is therefore ideal in situations where physical effort is frequently required to push equipment along. TENTEprene protects not only the floor but also the health of the employees.