C
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
C

9 Bejegyzések ebben az enciklopédia kategóriában

CAD: Computer Aided Design

The acronym CAD stands for Computer Aided Design. This means creating product graphics using a computer program. Both two and three dimensional drawings can be produced.
További információk

Castor and wheel requirements in intralogistics

The demands placed on castors and wheels in intralogistics are very high. The internal transport of goods needs to be safe, economical and efficient. 
További információk

Castor housing

A castor basically consists of three important components: the wheel, the fitting and the castor housing. But what is the difference?
További információk

Castor manufacturers

Stay on the move with TENTE, the castor manufacturer
További információk

Castor swivel bearing

Manoeuvrability and flexibility are the most important advantages when using practically any castor. The swivel bearing or back bearing determines how easily and smoothly this works.
További információk

Castors

Hardly any other invention has influenced the world as much as that of wheels and castors. Industrialisation, globalisation and much more. But what exactly are castors?
További információk

Castors for office chairs

The choice of castor for an office chair depends primarily on the type of floor:
További információk

Chemical resistance of castors and wheels

If castors or wheels are likely to come into contact with aggressive substances, their chemical resistance must be taken into account when selecting the right product.
További információk

Corrosion resistance of castors and wheels

Mobile devices are often used outdoors or in extreme conditions. In such cases, the corrosion resistance of the castors and wheels becomes important. The surfaces of the individual components must be appropriately treated to ensure that they are protected against corrosion.
További információk