W
What’s a plain bearing?
  • Продукти
  • Галузі
  • Рішення для мобільності
Лексикон: W
Washable castors to comply with strict hygiene regulations
Waste collectors: the right castors for smooth operation
What are lubrication nipples?
What are pneumatic tyres particularly suitable for?
What are rubber tyres?
What are the advantages of a polyurethane tread?
What are the advantages of a rubber tread?
What are the advantages of central locking?
What are the advantages of triangle dollies?
What are the properties of polyamide as a tread on wheels and castors?
What are the pros and cons of plastic castors?
What are thermoplastic elastomers?
What does ergonomics mean?
What does ESD stand for?
What does PAH stand for?
What does the RoHS directive regulate?
What factors influence the swivel resistance?
What is a guide castor?
What is a pallet truck?
What is meant by the resistance of wheels and castors?
What properties do solid rubber wheels have?
What requirements do industrial castors have to meet?
What’s a cone ball bearing?
What’s a drive wheel?
What’s a plain bearing?
What’s a plate fitting?
What’s a precision ball bearing?
What’s a stainless steel castor?
What’s a tugger train?
What’s central locking?
What’s important when choosing suitcase castors?
Wheels and castors
Workshop trolleys: Find suitable castors
A B C D E F H I L O P R S T V W
Початкова сторінка | Зміст
Навігація Lexicon
A B C D E F H I L O P R S T V W Початкова сторінка Зміст

What’s a plain bearing?

To ensure that castors always run smoothly, they require a first-class wheel bearing. The bearing is one of the factors that determines the running properties of the castor and is therefore an important characteristic of the quality of a castor. Different types of bearing are available to suit the various requirements that need to be met. The simplest of these is the plain bearing.

Plain bearing: Properties and applications 
Along with rolling bearings, plain bearings are among the most common types of bearing. Unlike rolling bearings, plain bearings have direct contact with the parts that move relative to each other. Plain bearings can be manufactured as plastic, metal or sintered bearings. They are low-maintenance or maintenance-free, impact-resistant and – depending on the material – also resistant to corrosion. These corrosion-resistant plain bearings have the great advantage that they can be used in wet operations, for example. 
The cost-effective plain bearings are particularly recommended for transporter equipment, which are only used at low speeds and over short distances. However, overheating problems can occur during continuous operation. 

Other types of wheel bearing 
In addition to plain bearings, the four most common bearing types include castor bearings, cone ball bearings and precision ball bearings. Each type of bearing has its own advantages, which come into their own in a wide variety of applications. We also offer further versions for special solutions. At TENTE you will find the optimum castor with the right wheel bearing for every application. If you have any questions about the different types of bearing, please do not hesitate to contact us – we will give you detailed advice and help you to choose the right wheel bearing!