Anika evo
Join us for a more sustainable future with castors and wheels
Environmental protection is important to all of us. It is for this very reason that TENTE wants to set an example and to leave a green footprint on our valuable planet. Therefore, we are proud to present: Anika evo – the first castor product range made of plant-based material. Anika evo is made of up to 98%* biomass materials originating from the castor bean. The Anika evo castor offers the same product quality and colour flexibility as the well-known Anika castor. In producing a sustainable furniture castor, TENTE is the first manufacturer ever to incorporate the caster bean into a furniture castor product range. The utilization of the castor bean helps us to reduce the carbon footprint by 46%**. TENTE´S DNA consists of developing and exploring new possibilities – product development for a more sustainable future is no exception. You can be a part of this sustainable journey!