Customer reference
Easy and safe picking so the belt keeps on moving
The employes at the engine production site should be able to push and stop their order picking trolleys easily. At the same time, the drive unit should be easy to handle and to maintain. For this purpose, NoBa Solution GmbH used the E-Drive system from TENTE. The hand control can be easily operated with one hand. The other hand can be used to operate the scanner or the iPad for order picking.
NoBa Solution slowed down the speed of TENTE‘s E-Drive system to 4 km/h. This way, even if a worker bumps into the trolley up front, the trolley will stop automatically without causing any injuries. A foot protection in front of the casters also prevents potential accidents.
Florian Bauer, Shareholder and Managing Director of NoBa Solution GmbH
By providing automatically adjustable working stations and by installing the E-Drive from TENTE in the picking trolleys, the employes benefit from ergonomic operation. Now the employes of the engine company can easily push and stop their trolleys without having to bend down to load the trolleys.
In this way, an ergonomic work process has been developed that preserves the health and performance of the employes.