There are practically no limits to the design possibilities for our caster surfaces. Different coloring methods are used depending on the requirements profile: printing, coating and complete through-coloring.
We have three different methods just for printing the caps: Laser printing offers different shades of grey and is therefore ideally suited for printing logos and text. Pad printing allows any colour insert, so that logos and symbols can be reproduced in color. UV direct printing has no colour restrictions either, and is particularly recommended for displaying images. The coating process can be used to give the forks and housing of the castor an individual and high-quality surface finish – also using special coatings, on request.
Not only the color shade and printed image, but also the gloss level can be defined, depending on the process. Complete through-coloring of the plastic offers the greatest possible resistance to mechanical influences during use. In addition to homogeneous coloring of the components, different degrees of gloss and surface texture requirements can be individually implemented at tool level.
Our solutions
Contact
Are you interested in individual solutions?
Contact us - we look forward to provide advice
TENTE Casters, Inc.
2266 Southpark Drive
Hebron KY 41048
United States
Phone: +1 859 586 5558
Email: sales.us@tente.com