Safety Casters
How to reduce the workload of doctors and nurses without compromising patient safety? Through the use of surgical robots
You have probably encountered the problem of overcrowded hospitals. One reason for this is demographic change, which is leading to an increase in the average age of patients and nursing staff. Unfortunately, there are also hardly any new specialists coming in and the shortage of skilled workers is increasing. This is because the high workload discourages new employees. This fact alone puts an enormous pressure on hospitals. On top of that, doctors are constantly being asked to perform at their best. Operations are becoming more complex and more frequent. Due to operations lasting several hours in ergonomically poor postures, doctors often suffer from side effects of surgery, such as limb and joint pain. The result is physical limitations for the doctors and a hazard for the surgery patients. A solution is needed, and that solution is: surgical robots.