The tread material has a profound influence on the quality of a castor or wheel. It influences the smoothness of running, the resistance – starting, rolling and swivel resistance – and the drive comfort of the castor or wheel.
All rubber treads dampen vibrations and are generally extremely gentle to floors. They have low swivel and roll resistance, which means excellent operating comfort. Another advantage is the material's resistance to many aggressive substances. Solid rubber can be used almost universally. Heat-resistant solid rubber tires can be used even at extreme temperatures above 200 °C. Thermoplastic rubber is non-marking and runs quietly. However, this material cannot be used in the high temperature range.
Pneumatic tires are made of rubber. Their roll resistance is low even on difficult floors. In the case of pneumatic tires, it is important to maintain the specified tire pressure at all times. Regular pressure checks ensure the tires continue to function properly in the long term.
We can help you choose the best tread material for your casters and wheels. Whether it is rubber, polyurethane or any other material – we will find the solution that makes your application run smoothly!
Advantages of a rubber tread
;Rubber surfaces have in common that they are usually extremely gently to floors and dampen vibrations. They offer minimal swivel resistance- and roll resistance so that the driving comfort is high. Another advantage is the material's resistance to many aggressive substances. Solid rubber, for example, can be used almost universally. Heat-resistant solid rubber tires can be used even at extreme temperatures above 200°C. Thermoplastic rubber is non-marking and runs quietly. However, this material cannot be used in the high temperature range.
Pneumatic tires are made of rubber. Their roll resistance is low, even on difficult floor conditions. In the case of pneumatic tires, it is important to maintain the specified tire pressure at all times. Regular pressure testing ensures the tires are functional in the long term.
We can help you choose the best tread material for your casters and wheel selections. Whether it be rubber, polyurethane or any other material – we will find the solution that makes your application run smoothly!