Customer reference

Castors strong enough to hold 63,000 kilos.

Read more

63,000 kilograms is roughly equal to the weight of 18 small lorries.

This is also the weight that AVT Europe, a Belgian customer of TENTE that specialises in heavy good transportation needs to carry. When the company was looking for suitable castors for its new models, we were asked if we could provide a solution that would cope with such heavy loads. Our answer: “Will do,” we said.

The starting point

AVT Europe NV makes driverless heavy-load transporters for the movement of heavy goods such as aircraft parts or railway carriages. The transporters resemble massive mobile platforms and are fitted with intelligent electronics. They are operated by remote control and can carry loads of up to 100 tonnes.

Compact design, high load capacity

The weight of the load being transported is distributed evenly across all the castors with the aid of air cushions. In order to do so, these heavy goods transporters units are equipped with load-bearing castors and drive wheels. Specifically, the load-bearing castors are always in use and take on the main load. The drive rollers, by contrast, are designed to be lowered to the ground automatically, as and when needed, and they also help to set the transporters in motion.

For AVT, it is important that all the castors have a comparatively small diameter, yet can still withstand heavy loads of up to 12 tonnes while in motion and 20 tonnes while stationary. Outstanding quality and maximum durability play a decisive role in this. Supreme quality and excellent durability are also key factors because the transporters are supplied to various companies, including big names like Daimler, Airbus and the nuclear research institute, CERN. These companies need to provide a reliable transport service for extremely high-quality goods

The selective customers of AVT expect a lifetime of 20 years and a warranty of 2 years. Therefore, our task was to provide castors that meet this diverse set of requirements without any doubt.

Our smart mobility solution

To cope with the extreme operating conditions, our Omega quadro castors were used. These castors are characterised by their special design, which features two wheels to the left and two wheels to the right of the centre. This gives them a higher load-bearing capacity. However, at the same time, the point loads are low, which in return allows the applied weight to be better distributed over the larger contact area.

They are therefore particularly easy steering even under heavy loading. This is because the counter-rotation of the wheels around the common centre makes the rolling and pivoting resistance significantly lower than the resistance of castors containing just one wheel. This differential effect gives the Omega quadro incomparable agility.

The drive wheel was custom-made and developed in close cooperation with the AVT staff. The wheel has a diameter of 400 millimetres and an overall height of 500 millimetres. Another crucial advantage is that all the running surfaces are polyurethane, which is good for handling characteristics and easy on the floor. As a result of considering the entirety of the tasks at hand, we were able to provide AVT with an intelligent solution in which all components are perfectly coordinated with each other.

What convinced us was the durability of the special castors – as well as the know-how of our partners at TENTE.

Maarten Van Looveren, General Manger at AVT Europe

Excellent durability and rapid adaptation to market needs

The AVT heavy-duty transporters are capable of carrying goods with a total weight of 63 tonnes. The well-considered design of the wheels guarantees maximum durability and improved rolling resistance. This in turn enables AVT to install less powerful drives in its transporters and thus save costs and energy.

 

In addition, the company can also rely 100 percent on something else: us. Our employees in Belgium works closely with AVT and are on call to support the provider of heavy-duty transporters with any future special developments. We are extremely flexible and can therefore respond to the growth of the company. No doubt this is another reason why AVT is planning to use TENTE castors in its future projects.

Related Downloads

PDF

Related Downloads

Download

Our solutions

General information

Dynamic loading: A complex interplay of forces

Customer reference

Small castors can usually only carry a low weight – but this general rule doesn’t always apply

General information

Material science for heavy tasks

Contact

Are you interested in individual solutions?

Talk to us - we are happy to advise you

* Mandatory field

Solutions for your individual requirements. Do not hesitate to contact us personally.

Fahed H. Khanjer

Jordan

Phone: +96 2 27 24 39 36

Fax: +96 2 27 24 75 77

Email: info@tente.de