Customer reference

100 percent safety. – zero percent metal.

Read more

Anyone who has already held a magnet to a coin knows what forces can be unleashed.

MRI images in the hospital are similar. In order to obtain diagnostic images of the body, the device generates strong magnetic fields. Therefore, in certain MRI areas, only devices and furniture that do not contain magnetic components are permitted. For this reason, our customer RCN manufactures special MRI products and relies on a completely metal-free castor that meets the high safety standards: the TENTE Levina scan.

The starting point

RCN MEDIZIN- UND REHATECHNIK GMBH develops a wide range of products for everyday care. These include shower stools, wheelchairs and walkers. The company also offers chairs, infusion stands, couches and shelf units that are non-magnetic. These are especially recommended for use in the field of magnetic resonance imaging or, in short: MRI. The company has been producing nursing aids for more than 30 years and employs around 100 people in factories in the USA and Germany.

SPECIAL REQUIREMENTS

An MRI device generates high-resolution images and does not involve exposure to radiation. During tomography, electromagnetic fields, whose strength is measured in Tesla, are generated. MRI devices with up to three Tesla are standard equipment in hospitals. For greater accuracy of detail, doctors are increasingly using devices with higher Tesla values, which also generate stronger magnetic fields. This means that: magnetic objects are prohibited in the vicinity of MRI machines. Due to the enormous forces of attraction involved, they pose a threat to staff and patients. RCN therefore develops medical furniture that uncompromisingly meets the strict requirements in this field. This furniture is made of standardised white plastic tubing and has distinctive characteristics. RCN manufactures products made of plastic and brass for MRIs up to three Tesla. Castors containing this metal are also used in this Tesla range. Brass is used for ball bearings and mounting fixtures. However, for examinations from seven Tesla upwards, the approval requirements for furniture and equipment are a real challenge: even non-magnetic brass is not allowed. In some countries, they have special security gates, which sound the alarm when they detect residual magnetism, are even used before entry to MRI zones. RCN therefore also manufactures all-plastic products that do not contain any metal components. In order for these infusion stands, couches and chairs to guarantee safe mobility, RCN requires castors that meet the high specifications for this use.

Our smart mobility solution

For particularly powerful MRIs from seven Tesla upwards, we have developed a special variant of our Levina Scan for RCN with total locking. The remarkable thing about this solution: We have managed to dispense with brass even down to the mounting fixtures and particularly for the ball bearings.

The castor is made up entirely of components that are 100 percent plastic. The Levina scan therefore exhibits no residual magnetism and guarantees the highest level of safety in MRI imaging. Compared to solutions containing brass, it has a higher load-bearing capacity and can carry a weight of up to 80 kilograms. To offer even more safety and stability, we have also carried out individual adaptations.

The castor stems are adapted to the size of RCN's standard plastic tubes. In addition, we have secured the Levina scan with a plastic screw on the frame so that the stem cannot twist. The castor is available in 100 and 125 millimetre sizes, in a simple swivel castor or a swivel castor with a total lock.

The Levina scan stands for 100 percent. 100 percent synthetic material and 100 percent safety.

Volkmar and Michael Jung, Managing Directors of RCN.

International advantages and various applications

With the Levina scan, RCN has the perfect castor for MRI use. Although made entirely of plastic, it has an outstanding load-bearing capacity and stands for maximum safety. Due to its properties, it is also suitable for MRI rooms in which metal detector locks are used. The solution also offers valuable advantages for RCN's international business.

Each country has its own regulations governing the use of products in an MRI environment. The Levina scan is a completely metal-free product and can be used worldwide without any restrictions, meaning extensive research into country-specific regulations is no longer necessary. RCN can use the plastic castor not only in the MRI area, but also in research facilities or security gates at airports.

Related Downloads

PDF

Related Downloads

Download

Our solutions

General information

Ergonomics as a key factor: productive and healthy

General information

Inspiration for the markets

Customer reference

Working platforms with crucial special equipment: enhanced safety.

Contact

Are you interested in individual solutions?

Talk to us - we are happy to advise you

* Mandatory field

Solutions for your individual requirements. Do not hesitate to contact us personally.

International for Agencies

95 El Gomhorya st.

Kairo

Egypt

Phone: +20 2 5 90 09 18

Fax: +20 2 5 90 09 13

Email: ifa.gamal.co@gmail.com