Customer reference
Halved noise emissions - with the same load-carrying capacity
Developing and producing efficient logistic solutions for trade and industry are the hallmarks of GEBHARDT Logistic Solutions GmbH. The company is successfully managed as a family business in its sixth generation now and can look back on a more than 185-year history steeped in tradition. GEBHARDT employs around 500 people worldwide at five production sites and has established itself as the market leader in warehousing and transport solutions.
Thanks to these, the noise level of a loaded roll container can be reduced by an impressive ten decibels, which is perceived as halving the volume.
The load carrying capacity, which is identical to that of conventional wheels, remained completely unaffected. The trick behind it: our Syntech is a hybrid wheel. The wheel body and base are made of polyamide, while the core is made of elastic solid rubber.
This allows us to combine the advantages of a hard tread with the strength of a soft wheel. The combination of the two plastics results in optimum damping properties and thus, significantly reduces noise emission.
This also interested the customers of the logistics expert. For example, the whole-sale company Transgourmet mentions the low-noise delivery of goods in its sustainability brochure and highlights it as a special quality. However, our cooperation with GEBHARDT focused not only on running noises.
Due to our holistic view of the logistics challenges and the Syntech wheels, we also scored highly in terms of stability. After all, the specialist for logistic solutions puts its products to the test and simulates real conditions through extensive trials. For example, heavily loaded roll pallets are tested to overcome thresholds and obstacles, such as when forklift trucks bump into them. The wheels also have to withstand cold and heat, dirt and rainwater, as well as show no signs of weakness even in snow. Our Syntech wheels have passed all of these tests.
Norbert Götz, Purchasing Manager at GEBHARDT Logistic Solutions GmbH
The Syntech wheel has a service life more than twice that of hard-filled castors, which are used for an average of only two years. In contrast, the Syntech wheel is often used for up to five years.
This saves costs both in purchasing and maintenance and is another decisive reason why GEBHARDT relies on long-term cooperation with our company.
Talk to us - we are happy to advise you
Safety International General Trading & Contracting Co.
Shuwaikh Industrial Area No. 3, Street 17, Khalifa Jassim Str.
70653 Shuwaikh
Kuwait
Phone: +965 24833959
Fax: +965 24837306
Email: safetykt@safetykt.com