Skip to main content Skip to search Skip to main navigation
Welcome to our newly redesigned website!

Stiegelmeyer

Low-profile castors for hospital beds that defy theory.
Customer_Stiegelmeyer_1
Imagine for a moment you are looking at a hospital bed castor:
It has a certain size and height. However, this latter measurement depends on an intelligent overall design. In hospitals especially, this is particularly important, since safety considerations dictate that the height of the castor fitting should not be more than the castor diameter. It’s impossible really to retain the ideal wheel size and at the same time reduce the height – in theory, at least. But, in fact, we have managed to do so and, in the process, have supplied our customer Stiegelmeyer with TENTE Linea.

The starting point

The Stiegelmeyer Group specialises in the manufacture of hospital beds. Their portfolio additionally includes hospital furniture. In hospitals, it is important to enable a low mattress base position to enhance patient safety. Falls can have serious consequences, particularly for people of an advanced age. To reduce the risk of injury, hospitals rely on beds whose mattress bases can be lowered substantially, to a very low level.

Would you like to receive personal advice?

We look forward to your inquiry

It’s the overall height that matters

Half of all patients in hospitals are over 65 years old. It is to be expected that this trend will intensify in view of demographic change. This makes fall prevention a crucial factor. Stiegelmeyer developed the Puro hospital bed which enabled nursing staff to set the height of the mattress base to a particularly low level. The hospital bed castors contribute decisively to how low this level can be.

Our smart mobility solution

We have been a reliable partner of Stiegelmeyer for more than 60 years. And we were also able to deliver the ideal solution in the case of the Puro hospital bed: the Linea hospital bed castor. Its outstanding feature is a fitting that is barely higher than the wheel size. With a diameter of 125 millimetres, the total height of the castor is only 130 mm. Safety was just one of the decisive factors when developing Linea. It was also important for our engineers to take the overall hospital environment into account and to focus on all influential factors. This included the design, hygienic aspects, noise development and the running characteristics. This resulted in the use of two precision ball bearings to allow the hospital bed castor to swivel exceptionally easily. The central locking mechanism is also maintenance-free. When it comes to the appearance, the colour scheme of the low-profile castor can be matched to the adjacent components and the bed frames. The cover in the centre of the wheel offers further options for customising the castor. Additionally, smooth surfaces discourage dirt pick-up and are easy to clean. Also, since a hospital is primarily a place for rest and relaxation, the castor locking and release mechanism is much quieter than the one of conventional products.

Georgios Kampisiulis Kemmler, Managing Director, and Anja Kemmler, Shareholder of the Stiegelmeyer Group

Our two family-owned companies have been working together closely for almost 50 years now. That speaks for itself.

Georgios Kampisiulis Kemmler, Managing Director, and Anja Kemmler, Shareholder of the Stiegelmeyer Group

Improved safety

The low-profile Linea castor makes it possible to significantly improve the safety of patients in hospitals. Thanks to its minimal overall height, nursing staff can adjust the mattress base so that it is only 28 centimetres off the ground. The Linea twin wheel castor therefore makes a significant contribution to considerably reducing the risk of injury in hospitals.
This smart solution also ensures that the running characteristics are satisfactory across the whole Linea range. The hospital bed castors offer the same load-bearing capacity as models with a larger overall height and also effortlessly overcome thresholds and any uneven areas. They also meet the highest hygiene standards, excel through particularly straightforward operation – and prove their true greatness with its low overall height.