F
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
F

7 Posts in this encyclopedia category

Find castors for tool trolleys

Tool trolleys are ideal for both professional craftspersons and DIY enthusiasts – for transporting large quantities of tools easily from one place to another. 
Read more

Finding the right castors for hospital beds

Hospital beds are in constant use, have to be manoeuvred back and forth, sometimes through narrow aisles, and have to stand securely in the patient's room. In order to meet these requirements, hospital beds must be equipped with appropriate castors. 
Read more

Fit care beds with easy-running, washable castors

Falling out of the care bed is a major risk that can never be completely eliminated. And bacteria and germs can spread incredibly quickly in care facilities. These factors also make great demands on the care bed castors.
Read more

Fitting elements for every type of use

The performance of a castor or wheel depends heavily on the optimum fitting. The type of fitting required is determined by the design of the equipment to which the castors are to be attached. 
Read more

Fixed castors

Nothing will throw TENTE fixed castors off track
Read more

Foot protection for castors

The protection of personnel plays an important role in mobile castor applications. If feet should accidentally get under the wheels, serious injuries can occur. 
Read more

Furniture castors: What must be taken into account?

Furniture castors are used in living rooms as well as in offices. The must meet different requirements depending on where they are used. These depend on the type of floor on which the castors are used, for example, and on the loads that have to be carried. 
Read more
Go to homepage
TENTE-ROLLEN GMBH 
Herrlinghausen 75 
42929 Wermelskirchen
Germany
Legal Information
  • Imprint
  • Privacy Statement
  • General terms and conditions
  • Terms of use
  • Installation instructions
  • Product Liability
  • Change Privacy Settings
Contact
  • Contact
  • Career
  • Newsletter
Supplier
  • Purchasing
  • Terms and Conditions of Purchase
  • Supplier Portal
Popular Categories
  • Braked Swivel Castors
  • Heavy Duty Castors