T
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
T

12 Posts in this encyclopedia category

Temperature conditions are of great importance when selecting castors and wheels

The factors to be considered when selecting the most suitable castors or wheels for your application include the temperature conditions to which they will be exposed. 
Read more

The castor material determines the properties

The castor material must be selected according to the requirements that the castor needs to meet. Generally speaking: No material can meet all of the requirements equally well.
Read more

The innovation of castors and wheels

The constant innovation of castors and wheels is our goal.
Read more

The relevant DIN standards for TENTE wheels and castors

TENTE castors and wheels are always developed and tested in compliance with the latest DIN standards, which are drawn up by the European Committee for Standardization (CEN).
Read more

The right castors for industrial and outdoor areas

The floor conditions influence the decision regarding which castors to choose. The basic principle is – for hard floors, use soft castors, and, conversely, for soft floors use hard castors.
Read more

The TENTE order numbering system – Clear and simple

To make sure that you can easily find the right castors and wheels for your application, we have developed a clearly structured order numbering system for our products.
Read more

The wheel centre

After the wheel bearing with axle material and the tread, the wheel centre is the third component of each wheel.
Read more

The wheel tread material

The tread material used for wheels affects various factors: the drive comfort, the resistance of the wheels and castors to temperature, various chemical and other influences, and how floor-friendly they are. 
Read more

These factors influence the running noise

In order to find the quietest possible TENTE castors and wheels for your application, you should consider not only the quality of the castors and wheels, but also the hardness of the tread and the type of floor.
Read more

Total lock for castors

Equipment or applications with castors should be fitted with a locking system to ensure a secure footing when stationary. 
Read more

Twin castor

The twin castor: sturdy and kind to floors
Read more

Two-component solid rubber: Tread material for castors & wheels

As an alternative to solid rubber, castors and wheels or tyres can be produced with a tread made of two-component solid rubber. This tread combines a harder rubber with a softer rubber.
Read more
Go to homepage
International for Agencies
95 El Gomhorya st.
Cairo
Egypt
Legal Information
  • Imprint
  • Privacy Statement
  • General terms and conditions
  • Terms of use
  • Installation Instructions