Refine your choice





Hospital bed casters are one of TENTE's specialist areas. We have decades of experience in the field and as a result have an extensive range of products on offer. The casters have to meet particularly stringent requirements, due to strict hygiene regulations, for example. Hospital bed casters with sealed precision ball bearings can be cleaned on a regular basis – the materials used are able to withstand the majority of detergents and disinfectants. The sturdy casters are designed specifically for everyday life in a hospital and therefore run extremely smoothly: The outstanding roll performance is kind to the nursing staff's backs and makes their work significantly easier. The nursing staff receives even more assistance with e-drive. Moving heavy beds suddenly becomes effortless thanks to the built-in motor. In addition, all casters are fitted with central and total locks. The design of TENTE's hospital bed casters has already won several awards, including the Red Dot Design Award, the iF product design award and the Interzum award.