Contatti Career Online Shop Eventi Downloads Termini tecnici Chi siamo Responsabilità aziendale Notizie Locations
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
  • Online Shop
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
H
Heavy duty castors
  • Prodotti
  • Settori
  • Soluzioni di mobilità
Lexicon: H
Heavy duty castors
Heavy-duty wheels from TENTE
0-9 A B C D E F G H I L M N O P Q R S V
Pagina iniziale | Sommario
Navigazione del lessico
0-9 A B C D E F G H I L M N O P Q R S V Pagina iniziale Sommario

Heavy duty castors



Areas of applications: 
The applications for this heavy duty castor are very varied and include uses such as for the army or the transport of goods in factories. Other areas in which the castors are used are: • Airports • Ports • Factories In these wide-ranging applications there are many devices that can be equipped with the castors. These include among others: • Work platforms • Mobile stairs • Mobile cranes • Emptiable containers • Tugger trains 

Heavy duty castors make the transport of heavy goods very easy 
Their solid construction with a heavy steel or stainless steel housing allows the heavy duty castors to lift heavy weights. For example, they can withstand several hundred kilos or even up to twelve tonnes per castor. Despite these heavy loads, they are always easy and precise to manoeuvre, so you can safely move your heavy loads to their destination. 
With the smooth-running heavy duty castors, the transport of heavy weights suddenly becomes very easy. The castors are manufactured with a high-quality blue passivated surface finish that allows each of our castors to be used for a long time. 

A heavy duty castor for every situation
The TENTE heavy duty castors are available in various designs - for example as swivel castors with a total lock or directional brake. These variants are particularly suitable for heavy equipment that has to be manoeuvred often and in all directions. 
We also offer them additionally as fixed castors, which provide more stability and safe immobilisation. Find the right castor for your application - TENTE's friendly service staff will be happy to advise you on all questions regarding the material, properties and load-bearing capacity. 
We are happy to develop innovative special solutions according to your specifications. 

Certified safety thanks to regular long-term testing 
Safety comes first when transporting heavy weights, so the heavy duty castors must be made of absolutely reliable material. To ensure this, we constantly carry out rigorous long-term tests. The load is simulated by different weights - on different floors and under different influences. 
This is the only way to ensure that each of the heavy duty castors used is durable, reliable and of excellent quality. We guarantee maximum load capacity - because that's what our "strong" castors are all about.
Passa alla homepage
TENTE S.A.S.
11, Rue de l'Orme Brisé - Pringy
77986 St Fargeau Ponthierry 
France
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
  • Online Shop
  • Newsletter
Fornitore
  • Acquisto
  • Condizioni di Acquisto
  • Portale Fornitori
Popular Categories
  • Braked Swivel Castors
  • Heavy Duty Castors
Sociale
Copyright © 2025 by TENTE International GmbH. All rights reserved. Designed by TENTE International GmbH
Choose your location

Africa

Asia

Australia

Europe
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
Richiesta inviata correttamente
La richiesta non è stata inviata - si è verificato un errore. Riprova.