T
7 Publicaciones en esta categoría de enciclopediaThe castor material determines the properties
                        The castor material must be selected according to the requirements that the castor needs to meet. Generally speaking: No material can meet all of the requirements equally well.
                    
                
                                                        
                            The innovation of castors and wheels
                        The constant innovation of castors and wheels is our goal.
                    
                
                                                        
                            The wheel centre
                        After the wheel bearing with axle material and the tread, the wheel centre is the third component of each wheel.
                    
                
                                                        
                            The wheel tread material
                        The tread material used for wheels affects various factors: the drive comfort, the resistance of the wheels and castors to temperature, various chemical and other influences, and how floor-friendly they are. 
                    
                
                                                        
                            Tratamiento de superficie para resistencia a la corrosión.
                        Tratamiento de superficie para resistencia a la corrosión.
                    
                
                                                        
                            Two-component solid rubber: Tread material for castors & wheels
                        As an alternative to solid rubber, castors and wheels or tyres can be produced with a tread made of two-component solid rubber. This tread combines a harder rubber with a softer rubber.