The starting point
Service trolleys as part of the Disney world
Our smart mobility solution
Richie Okorie, Managing Director, SOROL GmbH
When it comes to individual colour design, TENTE leaves nothing to be desired.
Richie Okorie, Managing Director, SOROL GmbH
Perfectly adapted to the corporate design
With the Linea designer castor, SOROL GmbH realised design concepts with this quality are only possible with TENTE. No matter what Disney theme worlds are to be conveyed – our solution meets the highest design specifications. The colour nuances know no bounds. For example, we presented the designer castor in the typical silver look to represent the 1920s and 1930s. We also delivered it in the particular gold of a brand too. To top it all off, our engineers can offer maximum user-friendliness. The use of TENTE Linea as trolley castor means that service trolleys can be manoeuvred comfortably, even in the narrow corridors of cruise liners and, even in heavy seas, you will be thoroughly impressed with their high stability.