Ball bearings belong to the group of rolling bearings. They use balls as rolling elements between the outer and inner ring. Cone ball bearings are a subgroup of ball bearings. Castors with a ball bearing offer particularly good running characteristics compared to those with a plain bearing. The quality of a castor depends heavily on the type of wheel bearing as well as on the swivel bearing, the tread and the wheel diameter. The choice of bearing therefore plays an important role. A castor used in heavy-duty transport, for example, places different demands on a wheel bearing than hospital bed castors or castors for shopping trolleys.
Cone ball bearing: Removable and readjustable
The cone ball bearing in TENTE castors is unlike other wheel bearings because it is detachable. This means that they can be replaced, if necessary, to ensure continued operation. It is also possible to readjust the conical ball bearings if natural wear and tear causes axial and radial play to occur in the wheel bearing. The bearing can be adjusted by tightening the axle screw connection until the play is taken up.
The quality of a castor depends heavily on the type of wheel bearing as well as on the swivel bearing, the tread and the wheel diameter. The choice of bearing therefore plays an important role. A castor used in heavy-duty transport, for example, places different demands on a wheel bearing than hospital bed castors or castors for shopping trolleys.
The team from TENTE is pleased to inform you about castors and wheels
The type of wheel bearing most suited to your application depends, among other things, on the loads to be carried and the duration and speed of use. In our online shop, you can filter your search to show only wheels with the desired wheel bearing, so that all of the suitable products are displayed immediately. If you have any questions about conical ball bearings or any other type of wheel bearing, please do not hesitate to contact us – our experienced staff is at your disposal to give detailed advice.
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
TENTE SIA
Franču 1, Stūnīši, Olaines novads
LV -2117
Latvia
Phone: +371 67 607330
Email: kkirpitis@tente.com