Castors with a plastic tread are used, for example, on small items of furniture or in industrial applications. The castors can be equipped with various bearing types such as plain bearings, ball bearings or castor bearings, which means that they have different rolling properties and meet a wide range of requirements.
Advantages and disadvantages of plastic castors
Among the advantages of plastic castors is the hygiene aspect. TENTE castors with selected plastics, chrome-plated steel parts and stainless-steel components are washable and resistant to many cleaning agents. This means that they can be cleaned regularly without any problems, even in the long term, and thus comply with the strict hygiene regulations that apply in the food industry, for example, or in the medical and pharmaceutical sector.
A disadvantage of plastic, however, is that it is a non-conductive material. If the castors become charged due to friction, the resulting voltage cannot drain away and the next contact with the ground will lead to an electrostatic discharge, which can have dangerous consequences. To avoid this, TENTE’s plastic castors can be produced with additives to make them electrically conductive.
Different plastics for the tread: PA, PP, PUR
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
Safety International General Trading & Contracting Co.
Shuwaikh Industrial Area No. 3, Street 17, Khalifa Jassim Str.
70653 Shuwaikh
Kuwait
Phone: +965 24833959
Fax: +965 24837306
Email: safetykt@safetykt.com