The dynamic load capacity plays an important role for transport equipment. It represents the maximum permissible load that a castor or wheel can withstand when repeatedly in motion over a long period of time. A distinction must be made between dynamic and static load capacity. The latter describes the permissible load when the transport equipment is stationary.
The dynamic load capacity T per castor is calculated using the following formula:
T = (E + Z) / (n-1)
E = Dead weight of the equipment
Z = Payload
n = Number of castors or wheels
In this calculation, the number of castors or wheels is reduced by one. This is because transport equipment is seldom used on perfectly even floors. Often, the load is not distributed to all of the castors or wheels at the same time. In order to take this into account, the load capacity calculation is designed to cover these cases too.
Important factors for the dynamic load capacity
The calculation is based on standard conditions, i.e. moving straight ahead on level floors at walking speed with uniform load distribution and a moderate ambient temperature (15°C to 28°C). If the actual conditions deviate from these, the load capacity will change. The actual conditions must therefore be taken into account from the start. For heavy-duty castors that can carry particularly heavy loads, it is also important to add a safety factor to the formula: the greater the load, the greater the safety factor.
If you have any questions about dynamic load capacity or need assistance in selecting the right castors and wheels, we are happy to help you - just contact us!
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
Safety International General Trading & Contracting Co.
Shuwaikh Industrial Area No. 3, Street 17, Khalifa Jassim Str.
70653 Shuwaikh
Kuwait
Phone: +965 24833959
Fax: +965 24837306
Email: safetykt@safetykt.com