Our large selection of castors and wheels includes plastic castors, made of polyamide or polypropylene, for example. They are available as fixed castors, swivel castors and lockable swivel castors. With TENTE’s intelligent system solutions, your transport equipment always stays on track and can carry even heavy loads easily and efficiently.
Properties and applications of plastic castors
Plastic castors impress with their high load-bearing capacity and abrasion resistance as well as low rolling and swivelling resistance. They are often used in industrial situations where a high load capacity is required. Thanks to their low swivel resistance, they offer a high degree of drive comfort, which is particularly advantageous for heavy loads. If they are used at high temperatures, however, the load capacity is reduced. For high temperature ranges, we therefore offer specially developed heat-resistant plastic castors that still benefit from the good properties of the plastic even at extreme temperatures. TENTE also supplies washable plastic castors. These are particularly suitable for use in the food and pharmaceutical industries as well as in hospitals and nursing homes, since they comply with the strict hygiene regulations that apply there.
Individual and innovative special solutions from TENTE
TENTE is all about innovation: We are constantly striving to produce new developments, with which you can set your equipment efficiently in motion. We are also at your service when it comes to tailored special solutions. In close cooperation with you we design new plastic castors and wheels to meet your specific requirements. Feel free to contact the experts in our team – we look forward to your enquiry!
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
TENTE RUEDAS, S.A.
Calle Vilatort 6
08110 Barcelona
Montcada y Reixach
Spain
Phone: +34 93 5650737
Fax: +34 93 5643646
Email: info.es@tente.com