Mobile shop building systems are used in supermarkets, shops and airports, for example. In supermarkets, fruit and vegetable display racks are pushed into the cool store every evening, for example, while discounted promotional merchandise in fashion stores is carefully positioned to promote sales. At airport bookshops, the most popular books are displayed in front of the entrance for passengers to pick up for inflight browsing. The mobility and manoeuvrability of these systems must be guaranteed at all times, as well as a secure footing when stationary. This requires special castors for shop building systems.
Shop fitting systems – good running and safe standing
Shop fitting systems usually have to be manoeuvred in confined spaces. This requires swivel castors that can be moved in all directions. If inferior castors are used, more effort will be required to push the units. This, in turn, will have a negative effect on the health of employees. The castors should ensure good drive comfort and have a high load capacity. It must always be possible to move the shop building system, not only when empty but also when fully loaded. When determining the necessary load capacity, therefore, the total weight must be taken into account.
TENTE Linea combined twin wheels
The twin castors of the TENTE Linea combined series have a robust castor lock. The wheel lock and directional lock are completely separate from one another here. This ensures that the castor can be fully locked, but also runs smoothly when the lock is released. The castors have a polyamide wheel body and a polyurethane tread. Electrically conductive, stainless steel and washable versions are also available.
We will be happy to answer your questions about castors for shop fitting systems in detail – please contact our experienced team. If required, we are also at your disposal for developing innovative and individual special solutions.