Flanged wheels are used for transport equipment that runs on rails.
Flanged wheels
Flanged wheels are the type of wheels that are used on rails. On the inner side, i.e. the side facing the middle of the track, they have a vertical bead, the flange, which keeps them in line. The tread that rests on the track butts up to the flange. If two flanges are connected by a wheelset shaft, the entire construction is referred to as a wheelset.
TENTE flanges are manufactured in a very heavy version made of polyamide with a precision ball bearing. Polyamide has the advantage of excellent abrasion resistance and the capacity to carry heavy loads. It is also temperature-resistant from -40 °C to +80 °C, so that it can be used in a wide range of applications. Customised flanged wheels can be equipped with a keyway. Depending on the version, the load capacity of the flanged wheels ranges from several hundred to several thousand kilograms.
Uses for flanged wheels
The best-known applications for flanged wheels are, of course, railway trains, trams and underground trains that run on tracks. In addition, the wheels are used wherever transport equipment runs on rails. This includes, for example, mobile cranes and production lines in many industrial sectors.
For industries with individual requirements for flanges, we develop special solutions in consultation with you to meet your specific needs. We would be pleased to advise you about your requirements – contact us!
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
E.G. Kistenmacher & Co.
Germany
Phone: +49 40 236 985 0
Fax: +49 40 236 985 10
Email: frank.dreyer@kistenmacher.de