ESD stands for electrostatic discharges. Friction can cause an electrostatic charge to build up in equipment. If this charge cannot be dissipated, it will discharge the next time contact is made with the ground.
Dangers associated with electrostatic discharge
The phenomenon of ESD is well-known from everyday life and although it can be unpleasant, it is generally harmless. The situation is different, however, in industry or in medical facilities, for example. Here, electrostatic discharges can have dramatic consequences. In areas at risk of fire or explosion, for example, there is a risk that gases or dust may ignite. Also, sensitive equipment can be damaged during discharge – an effect which, especially in hospitals, should be avoided at all costs! In order to prevent this, special ESD-compatible materials, which can conduct the voltage into the ground, are used in these types of situation.
ESD-compatible materials
Plastics and rubber are insulators, i.e. non-conductive materials. In order to make such a material conductive, conductive materials such as graphite particles are added to it. This reduces the ohmic resistance and the material can then also be used in the more sensitive areas. TENTE’s ESD-compatible castors are available in numerous versions for a variety of different applications. If required, we can also develop individual special solutions for you, which are designed to meet your specific requirements. Feel free to contact us for advice from our castor experts!
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
Solutions for your individual requirements. Do not hesitate to contact us personally.
TENTE SIA
Franču 1, Stūnīši, Olaines novads
LV -2117
Latvia
Phone: +371 67 607330
Email: kkirpitis@tente.com