Product configurator



When heavyweight items have to be moved, you're dependent on sturdy, high-performance wheels that can withstand a load that could be several tons. TENTE has developed wheels using the highest-quality materials that can stand up to daily use under construction cranes, scaffolds or other heavy-duty applications without failing, and, in the worst case scenario, endangering human lives. It's for this reason that we at TENTE attach such great importance to safety: Our wheels undergo rigorous long-term tests where they have to prove they can withstand even the high stresses exerted by several hundred kilos. Depending on requirement, our wheels can be fitted with a plain bearing, for example, or the highest quality bearing type, a precision ball bearing. This makes for exceptionally low rolling resistance even when under extreme load. You can customize the wheel body and tread according to your individual needs. Our wheels can optionally withstand temperatures as high as 200 degrees Celsius without any problem.