A wheel consists of three parts – the wheel bearing with axle material, the wheel centre and the tread. The latter is the part of the wheel that comes into direct contact with the floor. The tread can be made of different materials. Different tyre profiles are also used. The various properties of a wheel also affect the load-bearing capacity, running quality and rolling resistance.
The tread material
A distinction is made between hard and soft
Softer materials include rubber and polyurethane (PUR). These are extremely kind to floors and can be used in many areas. In the case of polyurethane, a distinction is also made between the cast and injection-moulded versions. Cast PUR is of higher quality, whereas injection-moulded PUR is slightly easier to manoeuvre.
The tread profile
Tyre treads often have a round, flat or trapezoidal cross-section. When we compare wheels that have exactly the same properties but different profiles, we see that a change in the profile or contact area occurs when a load is applied, and this changes the starting and rolling resistance. The contact area is initially larger with a trapezoidal profile than with a round profile, but smaller than with a flat profile. As the load increases, however, there is a displacement of the contact surface. In general, the smaller the contact area, the less force is required to overcome the starting and rolling resistance.
With a wheel or tyre, a point load, which can be very intensive, can also occur due to a locking device. In order to avoid problems, here, a material with good resilience must be selected.
Contact
Are you interested in individual solutions?
Talk to us - we are happy to advise you
TENTE-ROLLEN GmbH
Herrlinghausen 75
42929 Wermelskirchen
Germany
Phone: +49 2196 99-0
Fax: +49 2196 99-221
Email: info.de@tente.com